Classes

Classes define the structure of the database and the tables within it. Each class consists of a collection of Fields, Aggregates, and Methods. The structure of a Tables is defined by the classes that form the table.

There are two types of class:

Each class has a base class except CDBObject and CAggregate (the roots of the class hierarchy).The base class is the parent class of the class.

The classes that are base-classes also have sub-classes. The sub-classes are the child classes of the selected class.

You can use the Geo SCADA Expert Database Schema to display information about each class (see Working with the Database Schema).


Disclaimer

Geo SCADA Expert 2020