Actions Associated with Scanners on Simple Drivers
The scanners on simple drivers support a combination of these actions:
- Acknowledge Alarms
- Acknowledge with Comment
- Alarm Response
- Cancel Refresh
- Disable Alarms
- Disable Scanner
- Display Points
- Enable Alarms
- Enable Scanner
- Refresh
- Release Exclusive Control—(Systems on which Exclusive Control is enabled)
- Remove Alarms
- Remove with Comment
- Reset Point Statistics
- Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
- Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled)
- Unacknowledge Alarms
- Unacknowledge with Comment.
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
For information on any scanner-specific actions that are not listed above, see the relevant driver guide.