Comms State Alarm

Associated with: Outstations, including Slave outstations

This status attribute indicates whether communications between the driver and the outstation is healthy.

Possible States: Displays one of the Standard Alarm States.

If this attribute displays an alarm condition, but the outstation’s Channel State Alarm attribute indicates a healthy channel, this suggests that Geo SCADA Expert has detected a problem with the outstation, rather than the channel.

Also see State.

For information on resolving communications problems, see Troubleshooting in the Geo SCADA ExpertGuide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2020