Comms Statistics

Associated with: Scanners; Slave sources; most channels on advanced drivers; outstations; Slave outstations

This status attribute displays statistics about the communications with or via a particular item. The information that the attribute displays varies, depending on the type of item with which the attribute is associated.

With a scanner on a simple driver, the statistics that are displayed vary, depending on the type of scanner—see the driver-specific documentation for details.

With a Slave source on a simple driver, the Comms Statistics status attribute displays the number of times that the SCADA master has successfully or unsuccessfully read data from that source.

Example:

10 good reads, 2 bad reads

With a channel on an advanced driver, the Comms Statistics status attribute displays the time period for which the various channel statistics apply. If the Reset Statistics pick action has been used to reset the channel’s statistics, two Comms Statistics entries are displayed—the lower entry lists the time period for which the previous set of statistics applies, the upper entry lists the date and time at which the current statistics commenced.

On a channel on which non-continuous polling is used, the Communication Statistics Updates fields on the Channel Form’s Scan Parameters tab specify when the statistics are updated (see Defining the Communication Statistics Update Rate in the Geo SCADA Expert Guide to Advanced Drivers).

Example:

Comms. Statistics Since 17/Mar/2008 09:24:46.116

Comms. Statistics Between 05/Dec/2007 10:12:05.296 and 17/Mar/2008 09:24:46.116

The actual statistics to which the time periods apply are listed below each Comms Statistics entry. Such statistics include a channel’s Message Count.

Direct channels on some advanced drivers support a Scan Statistics status attribute, rather than the Comms Statistics status attribute. The driver-specific documentation lists any such driver-specific channel attributes where this applies.

With an outstation on an advanced driver, the Comms Statistics status attribute displays information about the success, or otherwise, of the communications between the Geo SCADA Expert server and that particular outstation.

The attribute displays the number of:

If the Reset Comms Statistics pick action has been used to reset the statistics on an outstation, two Comms Statistics entries are displayed—the lower entry lists the previous communications statistics, the upper entry is ‘live’ and logs the communications statistics since the pick action was last used.

Example:

56 good messages, 5 unsolicited messages, 3 bad messages, 4 no replies, 0 errors, 54 polls since 18/Oct/2007 11:03:25:217

13560 good messages, 55 unsolicited messages, 13 bad messages, 34 no replies, 0 errors, 13547 polls between 05/Oct/2007 09:57:29.642 and 18/Oct/2007 11:03:25:217

(To ascertain similar statistics for all of the outstations on a particular channel, as opposed to the statistics for a single outstation, look at the channel’s Message Count status attribute.)

With a Slave outstation on an advanced driver, the Comms Statistics status attribute displays information about the success, or otherwise, of the communications between the Slave outstation (Geo SCADA Expert) and its SCADA master.

The attribute displays the number of:

Again, if the Reset Comms Statistics pick action has been used to reset the statistics on a Slave outstation, two Comms Statistics entries are displayed—the lower entry lists the previous communications statistics, the upper entry is ‘live’ and logs the communications statistics since the pick action was last used.


Disclaimer

Geo SCADA Expert 2020