Current M/S State

Associated with: Analog points on which Master Station Alarm Limits are used

This attribute is displayed in place of the Current State for analog points on which Master Station Alarm Limits are used (see Master Station Alarm Limits in the Geo SCADA Expert Guide to Core Point Configuration).

Use the attribute in conjunction with other attributes to assess the reliability of the point’s data.

(The possible states for a point are specified on a per-point basis, on the corresponding Point Form.)

Also see M/S Alarm Limits.


Disclaimer

Geo SCADA Expert 2020