Disable Outstation
            Associated with: Outstations
Security permission required to access this pick action: Disable Points
                        
Use this pick action to take an outstation Out of Service.
The Disable Outstation pick action clears the outstation's In Service property, so that the outstation is no longer active.
You might want to disable an outstation, for example, if Geo SCADA Expert has detected a problem with that outstation. Once the problem has been rectified, use the Enable Outstation pick action to place the outstation back In Service.
Geo SCADA Expert logs an entry in the Event Journal whenever either pick action is used. The entry indicates whether the outstation has been enabled or disabled.
Be aware that disabling an outstation also de-activates its dependants, although their configuration will remain unchanged. Dependants include items such as points and pulse actions that are associated with the outstation. Additionally, if the outstation that you are disabling acts as a 'parent' outstation to one or more remote outstations, communications with those remote outstations will cease if no other communications route is available.
If using this pick action with the Automation Interface, you need to specify the method name Disable.