Disable Server
Associated with: Servers
Security permission required to access this pick action: Disable Points
Use this pick action to take a server Out of Service.
The Disable Server pick action clears the server's In Service property, so that the server is no longer active.
You might want to disable a server, for example, if Geo SCADA Expert has detected a problem with the device that the server represents. Once the problem has been rectified, use the Enable Server pick action to place the server back In Service.
Geo SCADA Expert logs an entry in the Event Journal whenever either pick action is used. The entry indicates whether the server has been enabled or disabled.
Be aware that disabling a server also de-activates its dependants, although their configuration will remain unchanged. (Dependants include items such as the scanners and points that are associated with the scanner.)
If using this pick action with the Automation Interface, you need to specify the method name Disable.