Last Good Incoming Call

Associated with: PSTN outstations or outstations on which PSTN fallback is enabled

This attribute displays the date and time of the last successful call that the outstation made to Geo SCADA Expert. The attribute displays the time at which the call commenced.

The information is updated whenever an incoming call completes successfully.

Example:

20/Mar/2008 12:41:08.140

Also see the Incoming Calls attribute, which provides a summary of the incoming calls since the statistics were last reset.


Disclaimer

Geo SCADA Expert 2020