EXP
The EXP function is a mathematical function that returns the base of natural logarithm raised to a power (en).
Function Name | EXP |
Description |
Returns the base of a natural logarithm raised to a power (en) |
Arguments |
EXP(INTEGER or REAL) The input value can be an integer or a real floating value—see Number (Integer or Real). |
Returns |
INTEGER or REAL (same data type as input). |
Example:
EXP(2)
The output is 7.39