Selecting a Mimic Parameter

To insert a Mimic parameter in an expression:

  1. On an Expression display for the Mimic, move the cursor to the position in the expression where the Mimic parameter will be entered.
  2. Select the browse button to display a context-sensitive menu.
  3. Each of the Mimic's parameters are shown in the menu (between the options for tags and colors). If the Mimic has no parameters, there are no parameter options shown.

  4. Select the option for the required parameter, for example, if you want to insert a Mimic parameter named 'CurrentStateDesc', select the CurrentStateDesc option.
  5. Select the OK button to close the Expression display and confirm your selection.

For information on entering a Mimic parameter manually, see Syntax of a Mimic Parameter Tag.


Disclaimer

Geo SCADA Expert 2020