Working with the Expression Window

When you have displayed the Expression window, you can use it to create expressions for:

The Expression window consists of check boxes, an Expression work area, and a browse button.

Some check boxes are specific to the type of item you are configuring. The Expression window for Mimics provides a Hover check box and a Fast Updates check box that are not shown on the standard Expression window.

The image below shows the standard Expression window:

You can use the various features of the Expression window as follows:


Disclaimer

Geo SCADA Expert 2020