Group n Interrogation Alarm

Associated with: IEC 60870-5 outstations

Each of these attributes indicates whether the latest attempt to scan that particular group of points for current data has been unsuccessful. One Group n Interrogation Alarm attribute is displayed for each of the 16 possible interrogation groups.

The frequency with which Geo SCADA Expert attempts to scan each group of points for current data is specified as part of the outstation’s configuration (see Configure the Station and Group Interrogation Intervals).

Possible states: Displays one of the Standard Alarm States. (Unused groups display the state ‘Enabled Inactive’.)

Further Information

Understand and Resolve Outstation Interrogation Alarms.


Disclaimer

Geo SCADA Expert 2020