Typical Identification Values for KEMA points
The following table lists the defined data types for KEMA points and the corresponding Type Identification Values.
Type of Measurement | Type Ident. Value | Data type description |
---|---|---|
Analogue values | 9 | Measured value: normalized value |
10 | As above with time tag | |
11 | Measured value: scaled value | |
12 | As above with time tag | |
Digital command | 45 | Single command |
Analog command | 48 | Setpoint command: normalized value |
49 | Setpoint command: scaled value | |
Digital status | 1 | Single point information |
2 | As above with time tag | |
Counter values | 15 | Integrated total |
16 | As above with time tag |