Configuring a Kingfisher Outstation Set
The Kingfisher driver supports these types of Kingfisher outstation set:
- Kingfisher Direct Outstation Set—A set in which the outstations use a single direct channel to communicate with the server.
You need to configure one Kingfisher Direct Outstation Set for each group of Kingfisher outstations that communicate via a particular direct channel.
- Kingfisher Shared Outstation Set—A set in which each outstation can communicate with the server using either of two direct channels. Each outstation in the set can use either channel.
You need to configure one Kingfisher Shared Outstation Set for each group of Kingfisher outstations that communicate via, and share, a particular pair of direct channels. For an example of Shared Set usage, see Kingfisher Master Outstation using a Shared Outstation Set.
- Kingfisher Switched Outstation Set—A set in which outstations communicate with the server using one of two direct channels.
As there are two direct channels, one channel is used for communications and the other is a backup channel. Geo SCADA Expert will switch the outstations from one channel to the other channel:
- If Geo SCADA Expert detects that the channel being used by the outstations has failed
- If Geo SCADA Expert detects that a specific number of outstations that use the channel have failed.
You need to configure one Kingfisher Switched Outstation Set for each group of Kingfisher outstations that communicate via, and can switch between, a particular pair of direct channels.
Kingfisher outstations support master station switching of channels on switched sets.
- Kingfisher PSTN Outstation Set—For outstations that connect to Geo SCADA Expert via the telephone network, using an individual or shared dial-up modem.
You need to divide any PSTN outstations into groups and configure one Kingfisher PSTN Outstation Set per group (see Configuring an Outstation Set in the Geo SCADA Expert Guide to Advanced Drivers).
Specify the features of each set using the fields on the appropriate Kingfisher Outstation Set Form.
Each Form has several tabs. This section explains the driver-specific fields on the Kingfisher tab of each Form. For information on the fields on other tabs, see Tabs on Outstation Set Forms.
Use the Kingfisher tab to:
- Specify the Master Station Address
- Specify Whether the Outstation Clocks Run at UTC or Local Time.
- Specify a Local System ID (Outstation Set)
For information on the minimal amount of configuration that you can undertake to produce a functional Kingfisher Outstation Set, see Minimum Configuration.