Driver Logging
Driver Logging is useful for investigating unexpected driver behavior as it provides diagnostic information for specific aspects of the system. For instance, the Points logging option provides diagnostic information on the points on a particular driver.
Should you need to contact Schneider Electric for assistance with unexpected behavior on your system, you may be asked to produce Log files. Be aware that existing warranty and support arrangements determine the level of help that you receive should you need to contact Schneider Electric.
Those driver logging options that are typically required for investigating driver behavior are enabled by default. We suggest that the logging options are left at this default unless other logging options are specifically requested by Schneider Electric, or the default options are adversely affecting system performance.
For information on producing Log files and defining the Log file settings, see Driver Logging in the Geo SCADA Expert Guide to Server Administration.
For information on the driver log options that are available for the Kingfisher driver, see Common Advanced Driver Log File Options in the Geo SCADA Expert Guide to Advanced Drivers.