Specify the Communications Re-Establishment Delay

Use the Delay while outstation performs a reset field to specify the delay between resetting a Kingfisher outstation and restarting communications.

The delay stops any messages from being sent to the outstation while it is in the process of resetting, then establishing communications with the server.


Disclaimer

Geo SCADA Expert 2020