Selection
You can use selection functions to provide a single output from a selection of inputs. One of the inputs is used as the output for the function—the type of function determines which output is used. Selection functions are useful when you need a program to choose an appropriate value from several inputs.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.