CPLD Version
Associated with: Lufkin SAMS controllers
This status attribute indicates the version of the controller’s Complex Programmable Logic Device (CPLD). The attribute is displayed once the controller is or has been in communication with the server.
Also see Bootstrap Version.