Specify the Dynacard Stores that Store the Rod Pump Data
Use these fields on the Lufkin SAMS tab to specify the Geo SCADA Expert Dynacard Stores that store the rod pump readings:
- Surface Dynacard Store—Specify the Dynacard Store that is used to store the pump’s surface readings.
- Downhole Dynacard Store—Specify the Dynacard Store that is used to store the pump’s downhole readings.
With each of the above fields, select the browse button to display a Reference browse window. Select the required Dynacard Store from the window.
Further Information
Dynacard Stores in the Geo SCADA Expert Guide to Advanced Drivers.