Specify the Gauge Off Time
            Use the Gauge Off Time field on the Lufkin SAMS tab to define the start of the working day. The property also defines the time at which Geo SCADA Expert updates the following point values in the database:
- The value of the analog point that provides a 24 Hour Historic data reading
 - The value of the analog point that provides a 60 Day Historic data reading.
 
Either use the spin box to select the required time, or overtype the entry (remembering to use 24-hour clock settings).