Configure the General Broker Properties
Use the fields at the top of the Broker tab to configure these properties:
- In Service—Use to specify whether the MQTT Broker item is active or inactive (see Placing an Item In Service).
If you take an MQTT Broker item out of service, its dependents (such as database points) also become out of service (although their configuration remains unchanged).
- Confirm Disable/Enable—Users with the required permissions can disable an MQTT Broker item that is In Service, or enable an MQTT Broker item that is not In Service. Such actions are carried out using the Disable Broker and Enable Broker pick actions.
Use the Confirm Disable/Enable combo box to specify whether a confirmation dialog box is displayed whenever an operator requests that this MQTT Broker item is disabled or enabled (see Requesting Confirmation of Action Requests).
You use the Disable Broker pick action to take an MQTT Broker item out of service. When an MQTT Broker item is taken out of service, its dependents (such as database points) also become inactive.