Add Comments for Custom Pick Actions and Menus

You can add a comment for your custom pick action menu. The comment will be displayed in the status bar when the cursor is positioned over the pick action menu in Run mode.

To add a comment:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Select the required action or menu.
  3. Enter the required comment in the Comment field.
  4. Select the OK button to confirm.

The Comment field works in the same way as the PickComment field on the Pick Action Configuration Wizard. For more information, see the relevant Pick Action Configuration Wizard section, for example, refer to Hyperlinks for information on the pick comment for a hyperlink pick action.


Disclaimer

Geo SCADA Expert 2020