Associating Mimic Objects with Pick Actions

You can associate any object on a Mimic with a pick action menu (a context-sensitive menu that provides access to specific options).

There are several types of pick action menu available, including:

You can set up any of these pick action menus. Geo SCADA Expert includes a Pick Action Configuration Wizard which you can use to configure pick actions. The Pick Action Configuration Wizard is a special display that contains a series of pages, each with specific settings. It is specially designed to guide you through each step of the pick action configuration process.

To learn how to display the Pick Action Configuration Wizard, see Accessing the Pick Action Configuration Wizard.

To remove a pick action association that has already been configured, see Removing or Disabling a Pick Action Association.

You can also use the Animations window to set up pick action menus (see Using the Animations Window to Set Up Pick Actions).


Disclaimer

Geo SCADA Expert 2020