Displaying the Parameters Window

You need to access the Parameters window if you want to add, edit, or remove a Mimic parameter.

To display the Parameters Window:

  1. Display a Mimic in Design mode.
  2. Select Parameters in the View command group on the Graphics Tab.

    The Parameters window will display.

The Parameters window lists Mimic parameters (if any have been configured) under these headings:

The Parameters window also contains these buttons:

There is also a Test Value field that you can use to check that the parameter is working as you expected. Simply enter a suitable value to see how the parameter will use the value. For example, if you have set up a parameter that uses a color value, when enter a number (0-255) in the Test Value field the Mimic item that is associated with the parameter should change to the appropriate color. The settings you enter in the Test Value field are purely for test purposes—they are not stored.


Disclaimer

Geo SCADA Expert 2020