Editing a Line

When you have added a line to a Mimic, you can access its Properties window to edit its settings. The line's Properties window is called the Polyline Properties window. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Polyline Properties window has three tabs which contain the settings that allow you to:

When you have edited the line, you can close the Polyline Properties window.

Remember that you will need to save the Mimic to store the changes you have made. You can save the Mimic by selecting the Save command on the Quick Access Toolbar or the File menu.


Disclaimer

Geo SCADA Expert 2020