Editing an Embedded Mimic

When you have added an embedded Mimic to a Mimic, you can access its Embedded Mimic Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Embedded Mimic Properties window has only one tab—the General tab. The tab contains Name, Visible, Animations, Pick Actions, ToolTip, and Dynamic Position settings that work in the same way as on other General tabs (see General Tab). However, the General tab on the Embedded Mimic Properties window also contains some settings that are specific to embedded Mimics. For more information concerning each setting, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020