Link to a Web Page by using the Pick Action Wizard

You can use the Pick Action Wizard to configure a hyperlink action for a Mimic object. This will allow the object to act as a ‘trigger’ - when selected, it will cause another display, in this case, a web page, to be shown.

When using the Pick Action Wizard to configure a hyperlink to a web page, you need to choose Hyperlink as the type of pick action and then define:

For more information, see Using the Pick Action Wizard to Create a Hyperlink.

Further Information

Using Animations to Create a Hyperlink.


Disclaimer

Geo SCADA Expert 2020