Configuring a Mitsubishi Scanner
            
            A Mitsubishi Scanner is logical functionality that runs within Geo SCADA Expert and scans for data on a Mitsubishi PLC or a Mitsubishi Slave.
Configure the Scanner properties using the fields on the Mitsubishi Scanner Form.
The Form has several tabs (see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers).
This section covers fields on the Scanner tab that are specific to the Mitsubishi driver (see Configure the Scanner Properties). For fields on the other tabs, see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers.