Configure the Historic Data Storage Properties

This section applies to ODBC Analog and Digital points.

Use the fields within the Historic Data Filter section of the ODBC tab to specify the type of data that Geo SCADA Expert is to store historically for the point.

Use the Historic Data Filter section in conjunction with the Historic tab, which defines whether the server stores values historically for the point, and whether any unnecessary data is filtered out to reduce storage requirements (see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration).

The Geo SCADA Expert server retrieves and processes the current data values from the devices that it monitors. Use the check boxes within the Historic Data Filter section to specify the type of retrieved data that Geo SCADA Expert is to store historically for a particular point:

If neither check box is selected, regardless of whether historic is enabled on the point’s Historic tab, Geo SCADA Expert will not store retrieved point values historically.


Disclaimer

Geo SCADA Expert 2020