Value Lookup

Use the fields within the Column Match Lookup section of the ODBC tab to specify the requirements for extracting data by reference to a specific value, such as a point name or ID. The fields are available for use when you specify a Value Lookup Method (see Configure SQL Query Lookup Properties).

For an example of how a point might be configured to extract data from an ODBC Query results table using the Value Lookup Method, see Query an Oracle Database using the Value Lookup Method.


Disclaimer

Geo SCADA Expert 2020