Configure the Scanner Properties
Use the fields on the Scanner tab to define the driver-specific properties of a scanner. Many of these fields are common to various scanners (see Configuring Scanners on Simple Drivers in the Geo SCADA Expert Guide to Simple Drivers). Those fields that are specific to scanners on the Simple OPC driver are described below.
- Server—Use the browse button to select the name of the server on which the OPC scanner is to scan data.