Use Custom Hyperlinks on a Mimic on a WebX Client

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of Geo SCADA Expert. For information about the Virtual ViewX client that is supported by Geo SCADA Expert 2019 onwards, for which the web server is hosted using IIS, click here.

Your system may include Mimics that have been configured with custom hyperlinks that, when selected, either:

or:

Example:

A pump on a Mimic is configured to display a ‘custom’ pick action menu.

A user selects the pump on the Mimic. The ‘custom’ pick action menu is displayed.

The user selects the required option. In this particular case, the Display Faceplate option.

The current Mimic display is replaced with one that shows specific status information about the database item, similar to that shown in ‘standard’ Status Displays.

For more information on custom hyperlinks, see the Geo SCADA Expert Guide to Mimics.


Disclaimer

Geo SCADA Expert 2020