Configuring Performance Monitor Server Settings

Some driver-specific settings need configuring on the server by a system administrator when a Geo SCADA Expert system is first installed. These settings are configured using the Geo SCADA Expert Server Configuration tool.

For information on how to access the Geo SCADA Expert Server Configuration tool, and for general information on server settings, see Configuring Simple Driver Server Settings in the Geo SCADA Expert Guide to Simple Drivers.

The rest of this section explains the settings that are specific to the Performance Monitor section of the Tool.

To monitor data, you need to use the fields within the Performance Monitor section to specify a suitable Windows user account. A suitable user account is required to enable the Performance Monitor driver to monitor performance data locally (on the machine on which you are configuring the settings) or remotely. The user account has to be a member of the relevant user group (for instance, the ‘Performance Monitor Users’ group). For more information on this and other requirements to enable Geo SCADA Expert to access performance data, see Accessing Performance Data.

ATTENTION: If you make changes on a server, you will also need to configure the same changes on the other servers in the system architecture (with the exception of permanent standby servers).

The User fields shown below are located within the Performance Monitor section of the Geo SCADA Expert Server Configuration tool:

You will need to restart the driver for any changes to come into effect (see Configuring Simple Driver Server Settings in the Geo SCADA Expert Guide to Simple Drivers).

If a user with insufficient privileges is specified in the fields above, a diagnostics message(s) is displayed, and either the affected scanners or points will display a Quality of ‘Bad’, or the driver will refuse to start and the Quality attribute will display ‘Device Failure’. (You can view Quality attributes in a Status display or on a List.) If this occurs, either adjust the user’s access privileges so that they are suitable, or specify the user name and password for a user that already has the necessary privileges.


Disclaimer

Geo SCADA Expert 2020