Specify the GSM Modem's Receiving Data SMS Messages Options
            Use the GSM Modems Receiving Data SMS Messages section on the SCADAPack 50 tab to specify the destination and type of the SMS messages sent by the device.
LOSS OF DATA
                
            
- Prefix Number—Specify a number prefix that the device should add to outgoing telephone numbers (if applicable).
 - Location Line n—Specify the destination to which the device should send SMS messages. This will  be a  local Geo SCADA Expert channel and/or a remote telephone number.  You can specify up to two destinations (Line 1 and Line 2). However, only one destination should be to a local Geo SCADA Expert channel, to avoid duplication of SMS messages in Geo SCADA Expert.            
Select a combo box option:
- Select Local for a local Geo SCADA Expert channel.
 - Select Remote for a remote telephone number. Remote in this context means remote from Geo SCADA Expert.
 
 - Channel—If you selected Local in the Location Line n field, specify the Geo SCADA Expert destination channel. Use the browse button to display a Reference window, and select a channel from the window.
 - Telephone Number—If you selected Remote in the Location Line n field, enter the remote telephone number to which the device should send SMS messages. For example, the remote Telephone Number could be a cell phone number, or the telephone number of a different SCADA system.
 - Phone Mode—Specify the type of SMS message that the device should send to the destination. Select a combo box option:
            
- Disabled. The device will not send any SMS messages.
 - Data and Alarm (SCADA Messages). The device will send both logged data and alarms.
 - Data Only (SCADA Messages). The device will send logged data only.
 - Text Alarm (Human-readable Messages). The device will only send text-based alarms.
			
If the destination is a Geo SCADA Expert channel, then you cannot select the Text Alarm option.
 
 
INOPERABLE DEVICE