Define the Set Clock Method
Use the Set Clock Method field on the SCADAPack tab to define whether a controller’s clock is synchronized from Geo SCADA Expert or another source:
The options vary, depending on the type of controller:
- None—The controller’s clock is synchronized via a source other than Geo SCADA Expert.
- TeleBUS—Geo SCADA Expert synchronizes a SCADAPack controller’s clock using a TeleBUS protocol command.
For information about any Set Clock Method options not mentioned above, see the appropriate SCADAPack Modbus extension driver guide.