SCADAPack Modbus Specific Status Display Attributes
            This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.
NOTE: This section is about status attributes that are specific to this driver. In addition to the status attributes mentioned here, this driver's extension drivers might support further status attributes. For information about driver-specific status attributes that are not covered in this section, see the relevant extension driver guide.
                
Further Information
Status attributes supported by this driver's parent driver: see Advanced Modbus Specific Status Display Attributes in the Geo SCADA Expert Guide to the Advanced Modbus Driver.