Supported SCADAPack Modbus Realfo Firmware Versions
Except where stated otherwise for specific features, this driver provides support for functionality that is available in SCADAPack Modbus Realflo devices that are running firmware up to and including the following version:
7
The earliest version of SCADAPack Modbus Realflo firmware with which the driver is compatible is 5.20.
For more comprehensive information about Realflo and Geo SCADA Expert cross-compatibility, see the Cross-Compatibility page on our Resource Center website. (The page also includes information about ClearSCADA, the name by which Geo SCADA Expert was formerly known.)