Compressibility Calculation Properties (Gas Flow Run)
            The Compressibility Calculation tab on the Flow Run Form displays the properties that are associated with a Gas Flow Run’s compressibility calculation. Use the fields to configure or view specific properties that are associated with the calculation.
The fields vary, depending on the The Compressibility Calculation Type that a Gas Flow Run performs.