Meter Input Properties
            The fields within this section of the Meter Input tab display those properties that are associated with measurement.
You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).
With Gas Flow Runs, properties are only displayed on the Meter Input tab if the Flow Calculation Type is set to AGA-11 (an option that is only available from Realflo version 6.95 onwards).
                
            
- Meter Input Type—Define the meter input type. The options vary, depending on the type of Flow Run, but will include a combination of the following meter input types:
			
- Mass flow
 - Mass (Pulse)
 - Volume flow (only available on Liquid and Water Flow Runs)
 - Volume (Pulse) (only available on Liquid and Water Flow Runs)
 
 
The availability of the remaining fields on the tab varies, depending on the Meter Input Type. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Further Information
For more detailed information on these properties, see the documentation provided with the Realflo application.