Realflo Specific Alarm and Event Categories
            Each alarm and event on a Geo SCADA Expert system has a Category that indicates the type of alarm or event. The Category is included by default in the Events List and, if applicable, the Alarms List and the Alarm Banner.
You can optionally filter the entries in either List by category—the entries from which you can choose comprise various ‘core’ categories, along with any categories that are specific to the drivers that are installed on your system.
On systems on which both the SCADAPack Modbus and Realflo driver components are installed, in addition to the ‘core’ alarm and event categories, these Realflo specific categories are available:
- EFM Alarm—Entries associated with EFM alarms that have been logged in the controller’s Flow Run.
 - EFM Event—Entries associated with EFM events that have been logged in the controller’s Flow Run.
 
Further Information
Events Lists and ‘core’ filter categories: see the Geo SCADA Expert Guide to Lists.
Alarms Lists and ‘core’ filter categories: see the Geo SCADA Expert Guide to Alarms.