Configure a Modbus Slave Device
You need to create a separate configuration item for each Modbus Slave Device that you want SCADAPack x70 to scan. A Modbus Slave Device configuration item allows you to configure and store the configuration settings on the SCADAPack x70 device. When you have created a Modbus Slave Device item use the Modbus tab to configure the settings.
You can add a maximum of 150 Modbus Slave Devices to a SCADAPack x70 device.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.