Minimum Configuration
For an SDI-12 Scanner to be functional (on-line), you need to:
- Specify the channel through which the scanner communicates
- Specify the scanner’s sensor ID
- The Data Length.
You also have to put the scanner In Service and save the configuration.
These are the minimum requirements and, when specified, will result in a scanner that uses the default configuration settings.