Define the Dynacard Poll Intervals

Use these fields on the SE RPC tab to specify the frequency with which Geo SCADA Expert retrieves dynacard data from the controller.

With each field, enter the interval in the OPC Time Format, or specify 0 to disable automatic polling.


If required, you can use the following pick actions between, or as an alternative to, scheduled polls:

For more information, see Actions that are Specific to the SE RPC Driver.


Disclaimer

Geo SCADA Expert 2020