Specify the Controller Address

Use the Address field on the SE RPC tab to specify the address of the SE Rod Pump controller. The address has to be unique on the system.


Specify a suitable address in the range 1 to 255.

Modbus uses address 0 for broadcasting, therefore this address cannot be used as an SE Rod Pump controller address.


Disclaimer

Geo SCADA Expert 2020