Conditions.bool-primary-between

Returns True if a value is between two given values

Format

expression [ NOT ] BETWEEN expression AND expression

Remarks

Checks if a value is between two given values. The range is inclusive.

y BETWEEN x AND z

is the same as

x <= y AND y <= z

y NOT BETWEEN x AND z

is the same as

NOT ( y BETWEEN x AND z )

Example:

CurrentValue BETWEEN ZeroScale AND FullScale


Disclaimer

Geo SCADA Expert 2020