NumericFunctions

This section describes functions returning a numeric value

Contents

Name Description
Absolute value expression Returns the absolute value of a numeric expression
Ceiling function Returns the next largest whole number
Exponential function Returns the value of e raised to the power of a numeric expression
Extract expression Returns a date/time field from a datetime or interval
Floor function Returns the next lowest whole number
Length expression Scalar functions to return the length of an item
Modulus expression Returns the modulus (remainder) of a number divided by another
Natural logarithm Returns the natural logarithm of a numeric expression
Position expression Returns the position of a substring within the given character or bit string
Power function Returns a number raised to the specified power
Regex occurrences function Returns the number of times a pattern occurs in another string
Regex position function Returns the position a pattern occurs in another string
Square root Returns the square root of a numeric expression

Disclaimer

Geo SCADA Expert 2020