StringFunctions
This section describes function returning a string value.
Contents
Name | Description |
---|---|
Character substring function | Extracts a substring from the given string |
Fold function | Scalar functions for changing the case of text strings |
Regex substring function | Extracts a substring from the given string using regular epxression pattern matching |
Replace function | Replaces all occurrences of string_exp2 in string_exp1 with string_exp3 |
Soundex function | Returns the Soundex code for a string expression |
Translate function | Returns the application dictionary translation for a string expression in the current user locale |
Trim function | Removes whitespace from a string |