Server

The Alarm.SelectedAlarms and Alarm.Alarms properties both return an alarm collection. The alarms in the alarm collection have a Server property that returns a Server object. In your script, you can access the Server object and its Server Functions and Server Properties.

Syntax

Server

Description

Represents the server on which the returned alarm has been raised.

Arguments

None.

Returns

Server.
The Server object has Server Functions and Server Properties that you can access in your script.

Example:

In this example, the script writes the values 123 and 456 into a data table’s Column A and Column B respectively. To achieve this, the script uses the Query property of the alarm collection’s Server property.

Dim sQuery

Set sQuery = Alarm.Server.Query("INSERT INTO DataTableName(ColumnA, ColumnB) VALUES ('123', '456')")

If sQuery.Error Then

MsgBox "Error inserting: " & sQuery.ErrorMessage

End If

DataTableName is the name of a variable that is defined elsewhere in the script. It represents a Data Table that is stored on the server that is represented by the server property.


Disclaimer

Geo SCADA Expert 2020