Archiving

The archiving feature allows you to provide long-term offline storage of Historic Types and Streams, event and configuration changes messages on a variety of devices (providing that storage and archiving of such data is enabled on your system), including:

You can access the historic data and events from the archives via Lists and Trends.

Restored historic data is only available on the server on which is it restored. In a Main-Standby setup, the restored data is only available on the Main or the Standby, depending on where the data was restored—the data is not restored across the link between servers.

ATTENTION: Any data that has been manually modified is permanently stored online it is not archived with the related historic data. However, when you access an archive, any related modified data is also shown.

For more information on modifying historic values, see Modify a Value on a Historic Trend.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Using Trends

Understand Historic Lists


Disclaimer

Geo SCADA Expert 2020