Considerations when Setting the Maximum Consecutive Read/Write Timeouts

When you configure the limits for the Maximum Number of Consecutive Read Timeouts and the Maximum Number of Write Timeouts, there are many factors you need to take into consideration:

Typically, you would look to increase the consecutive read and consecutive write timeouts if:

You may want to reduce the consecutive read and write timeouts if:

When you understand How Geo SCADA Expert Uses the Consecutive Read and Write Timeouts, and know about the Considerations when Setting the Maximum Consecutive Read/Write Timeouts, you can proceed to Change the Maximum Number of Consecutive Read/Write Timeouts.


Disclaimer

Geo SCADA Expert 2020